Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the LADN__ auxiliary contacts positive guided?
Issue:
Is the LADN auxiliary contacts mechanically linked when used on TeSys D contactors?

Product Line:
Tesys D line contactors and accessories

Environment:
Products sold and used in the United States

Cause:
Positively guided auxiliary contact needed

Resolution:
The contacts are all mechanically linked and when used with the D-Line contactor they are also mechanically linked with the contactors power poles and are suitable for use in category 4 safety circuits.