Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the 8903LG, LXG Nema 1 enclosures have the feature of being able to be padlocked ?
Issue:
Can 8903L Enclosures NEMA 1 can be padlocked?

Product Line:
NEMA and Definite Purpse Contactors and Starters

Environment:
8903 Type L Lighting contactors

Resolution:
Yes, enclosure provides a hole in the bottom of the cover for padlocking, reference page 14-105 Digest 173 and figure 1 enclosure.