Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do the GV2__, GV3__ or GV7__ manual motor starters require a separate thermal overload relay?
Issue:
Thermal overload relay for the GV2 line manual motor starters

Product Line:
Contactors and Starters IEC

Environment:
IEC Manual Starters

Resolution:
The overload is an integral part of the GV line manual starters and they are adjustable. Separate overload is not an option.