Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many contact blocks can be mounted behind a single speed pushbutton operator in a 9001 SKYP pendant station?
Issue:
Maximum number of contact blocka that can be placed at the back of a single operator on the 9001SKYP pendant station.

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony 30 mm 9001 SK Plastic Push Buttons

Resolution:
Contact blocks can be mounted two side by side behind a single speed operator in a 9001 SKYP pendant station. They cannot be stacked.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings