Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a mounting base needed for an XACA pendant station to connect contact blocks to the XA2 cover mounted operators?
Issue:
Mounting base to connect contact blocks to the XA2 cover mounted operators

Product Line:
Push Buttons and Operator Interface

Environment:
XACA Pendant Station

Resolution:
No, It comes with a center mounting plate.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings