Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a pole be added to an existing 8903SPO11V02 3 pole 60 amp lighting contactor?
Issue:
Can you add a pole to a 8903SPO11V02? Customer needs to have 4 poles?

Product Line:
Nema Contactors and Starters

Environment:
Type S Lighting contactors

Resolution:
Yes you can but you also need to order a 4 pole coil for the contactor. This can also be obtained with the power pole by adding Form Y118 to the power pole part number

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings