Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the Secondary Ring Nut come with any of the 9001 type K, SK or KQ selector switch knobs?
Issue:
Secondary Ring Nut inclusion

Product Line:
30 mm Push Buttons

Environment:
Type K and SK Accessories

Resolution
No, the secondary ring nut (9001SK46) is not included with the part number for the knob only. It is included on the selector switch body
ex. 9001KS43 (includes the selector switch body, cam, secondary ring nut) Knob and contact block needed for it to be a complete assembly (and light module for illuminated version)

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings