Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum branch circuit breaker available for HOMELINE load centers?
Issue:
Product features of Homeline

Product Line:
Homeline load centers

Environment:
Branch breakers

Cause:
Application

Resolution:
The maximum HOMELINE branch circuit breaker is 50 amperes (single pole) and 200 amperes (two pole).

NOTE:
The maximum branch breaker cannot exceed the ampere rating of the load center.
The two pole, 150-200 amperes, branch breakers are restricted for use in HOMELINE load centers rated 150 amperes or greater, and they take up four spaces in the load centers.
Homeline branch breakers are different from the old replacement Homeline main breakers by using suffix BB (example: HOM2150BB).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings