Inquiry:
What is the catalog number for the replacement handle extension for the Powerpact M and P frame Circuit Breaker?
Product Line:
Powerpact MG, MJ, PG, PJ, PK, PL circuit breakers
Resolution:
S46998 is the short handle extension (standard).
S46996 is the long handle extension (optional).
NOTE that the breaker handle, the part that the extensions screw on to, is not replaceable. If it is broken, the breaker must be replaced.
Released for: Schneider Electric Canada