Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a GFI option for the breakers used in the NF panelboards? (EDB, EGB, EJB)

Article available in these languages: Spanish

Issue:
GFI option for the breakers used in the NF panelboards (EDB, EGB, EJB).

Product Line:
NF Panelboards, E Frame Circuit Breaker

Environment:
Products sold in North America


Resolution:
No, the EDB, EGB, and EJB circuit breakers do not come with a GFI option for people protection at 4-6mA.  They are only available with equipment ground-fault protection at 30mA (EPD).  These are only available in single-pole.

Note: NF EPD circuit breakers cannot be used on phase to ground less then 277V. These breakers are not suitable for a 208Y/120V application.

18 ka @480Y/277 Vac35 ka @480Y/277 Vac65 ka @480Y/277 Vac
15 AEDB14015EPDEGB14015EPDEJB14015EPD
20 AEDB14020EPDEGB14020EPDEJB14020EPD
30 AEDB14030EPDEGB14030EPDEJB14030EPD
40 AEDB14040EPDEGB14040EPDEJB14040EPD
50 AEDB14050EPDEGB14050EPDEJB14050EPD

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings