Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between a Vertical and Horizontal type Class 8736?
Issue:
Difference between a Vertical and Horizontal type Class 8736

Product Line:
NEMA Type S Motor Starters (8536 8736 8606)

Environment:
NEMA Starters

Resolution:
The vertical arrangement provides the reversing contactor mounted above the forward contactor, which provides a tall, narrow device configuration. The horizontal arrangement provides the reversing contactor mounted to the right of the forward contactor, which provides a shorter, wider device configuration.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings