Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can The RM4TR32 unit be used on a 480V nominal system?
Issue:
Using the RM4TR32 Phase Failure Relay on a 480V nominal system

Product Line:
RM4 Zelio Phase Measurement Relays

Environment:
Zelio Phase Measurement Relays

Resolution:
No. RM4TR32 will not work on 480V systems. It will always be tripped on overvoltage. RM4TR32 is obsolete.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings