Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the CH324N, series F5? (may be shown as F05)
Issue:
Repair Parts

Product Line:
Safety Switch - Canada

Resolution:
The replacement parts for the CH324N, series F5 (F05) are as follows. No other parts are available.
Complete Line Base - 4056703050 (1 required; includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
Line Base mounting screws - 4020546401 (6 required per line base)
Load Base Assembly - 4056677450 (1 required per phase; includes phenolic base, lugs, and fuse clips)
Load Base mounting screws - 4020546401 (2 required per load base)
Arc Suppressor Assembly - 4053922001 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - 4025116251 (per lug)
Lug Assembly mounting screw - 2140122240
Switch Mechanism - 4056678650
Switch Mechanism mounting screws- 2299940562 (2 required)
Handle Assembly - 4056663550
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Neutral Assembly - CSN20 (includes mounting hardware and bonding screw)
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings