Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an 8502 or 8536 Type SA, Series A coil be used in a Series B controller?
Issue:
Are the 8502 or 8536 Type SA, Series A coil interchangeable with the Series B controller?

Product Line:
Class 8502/8536 Type SA Contactor/Starter

Environment:
Products sold in Norh America

Resolution:
It is not recommended to use these coils interchangably. The coil may not function properly and overheat as Series A have different winding with the series B coil.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings