Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the CH362DS, series F6? (may be shown as F06)

!!!Confidential ContentIssue:
Current design repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Resolution:
The repair parts for the CH362DS, series F6 (F06) are as follows. No other parts are available.
Line Base Assembly - 4056603850 (arc suppressor not included)
Load Base Assembly - 4056604050
Line & Load Base mounting screw - 4020515101 (3 for line & 2 for load)
Arc Suppressor Assembly - 4056635550
Arc Suppressor mounting screw - 4020514501 (1 required)
Lug Assembly - 4025101652 (per lug)
Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
Handle Coupling - 4056699850
Cover Interlock Defeat Coupling - 4056699750
Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
Lockplate mounting screw - 2194918121 (2 required)
Ground Lug - 4025101652 (2 required)
Ground Lug Mounting Screw - 4020513503
Fuse Pullers - FPK0610 (1 required)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings