{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the repair parts for an 82355, series A1 double throw safety switch?
Issue:
Repair parts

Product Line:
Double Throw Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Blade assembly - 4053859650 (3 required)
Top switch base assembly - 4053859550 (3 required)
Bottom switch base assembly - 4053859350 (3 required)
Base mounting screws - 2142718241 (2 required per base assembly)
Handle knob assembly - 4028435750
Lug assembly - 4025113651 (1 required per base assembly)
Keps nut for mounting lugs - 2342702200 (1 required per lug)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: