Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to mount the LRD** overload directly to the LC2DT** contactor?
Issue:
Mounting LRD** overload on LC2DT** contactor

Product Line:
IEC Contactors and Starters

Environment:
TeSys D Contactors

Cause:
Selection

Resolution:
It cannot be directly mounted on an LC2DT**. They will have to separate mount the overload and will need the LAD7B10 mounting kit to mount the overload. The overloads are set up to be mounted directly to the 3 pole contactors not the 4 pole.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings