Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the voltage codes for the TeSys K Line Contactors?
Issue:
What the 3 indicate in at the end of a TeSys K line contactor part number?

Product Line:
TeSys K contactors and accessories

Environment:
North American Products

Cause:
Product Selection

Resolution:

The AC voltage codes for the LC1K LC2K are listed below.
For integral suppression add 2 to the end of the voltage code, for example a 12VAC coil with integral suppression is J72.
AC Voltage12244248110120127200/208220/230230230/240277380/400400/415440480600
CodeJ7B7D7E7F7G7FC7L8M7P7U7UE7Q7N7R7T7X7

The DC voltage codes for the LP1K LP2K are listed below.
For integral suppression add 3 to the end of the voltage code, for example a 12VDC coil with integral suppression is JD3
DC Voltage12202436486072100110125200220230240250
CodeJDZDBDCDEDNDSDKDFDGDLDMDMPDMUDUD

The DC voltage codes for the LP4K LP5K are listed below.
These devices have built-in transient suppression.
DC Voltage12244872
CodeJW3BW3EW3SW3

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings