Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a retaining kit that will work on a single pole QO or Homeline circuit breaker?
Issue:
What is the retaining kit for single pole QO or Homeline circuit breaker?

Product Line:
QO Load Centers, Homeline Load Center

Resolution:
No, there is no retaining kit for a single pole breaker. The QO and Homeline load centers are 120/240 V single phase load centers. The panels are designed and tested using a 2 pole breaker feeding both phases of the panel, so there is no UL approved retaining kit for a single pole breaker in these panels.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings