Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a viewing window be ordered for a combination starter?
Issue:
Is there a combination starter with a viewing window.

Product Line:
8538, 8539 Combination Starters

Environment:
NEMA Contactors and Starters

Resolution:
Addition of a viewing window to a NEMA Type 1, 3R, 4 (SS Only), 12/3R combination starters can be ordered by adding Form ``G36``. The window will be on the front and is large enough to observe the status/position of the disconnect switch blades.
*****Applicable to Class 8538/8738 NEMA Size 0, 1, 2, 3 devices only.*****

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings