Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the operating handle of an enclosed circuit breaker in a M800S circuit breaker enclosure be padlocked in the ON or OFF position?
Issue:
Can the operating handle of an enclosed circuit breaker in an M800S circuit breaker enclosure be padlocked in the ON or OFF position?

Product Line:
Circuit breaker enclosure

Environment:
Padlock feature

Cause:
Feature clarification

Resolution:
The operating handle can be padlocked in the OFF position only by purchasing and field installing an S44936 Handle Padlocking Device. The S44936 is considered a ``removable`` device. The operating handle can be padlocked in the ON or OFF position by purchasing and field installing an S32631 Handle Padlocking Device. The S32631 is considered a ``fixed`` device. The external 9.25 x 9.25 cover plate must be removed to install and use the S32631.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings