Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the Powerpact P frame breaker available with ground fault alarm only, without tripping?
Issue:
Ground Fault Alarm only

Product Line:
Circuit Breakers

Resolution:
Use 5.0P (S163A) or 5.0H (S173A) trip unit and a M2C (S64273) or M6C (S64204). If replacing a standard trip unit (not A, P or H), the 12-pin connector for the trip unit (kit S33101 for Masterpact, S33100 for Powerpact) must also be ordered.

Set alarm up via trip unit Amperage Protection menu (trip curve button). Then set up S1 or S2 contact on 2PCM programmable contact module in MAINTENANCE menu (wrench button). Need neutral CT if it is a 4 wire system.

Example
See instruction bulletins.
Powerpact P, R, and Masterpact NW, NT Micrologic™ 5.0P and 6.0P Trip Units, see 48049-137-05
M2C Programmable Contact Module Kits, see 48049-227-02
M6C Programmable Contact Module Kits, see 48049-337-02

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings