Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a Field Installable Coil Transient Suppressor Available for 120 Volt Control coil on the 8903 Type L or LX Lighting Contactors?
Issue:
Suppression module for the Type L and LX lighting contactors

Product Line:
Contactors and Starters

Environment:
8903 Lighting Contactors

Resolution:
The 9999ST1 transient suppression module, while specifically designed for use with a Type S contactor, could be used for this application requirement but will require panel mounting. Please note that 8903 Type LX mechanically held devices require two modules, (1) for latch coil and (1) for unlatch coil.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings