Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does form Y243 mean when referring to 9001 type K or SK push-to-test pilot lights?
Issue:
How the Push-To-Test pilot lights cab be used in certain hazardous locations such as Class 1, Division 2?

Product Line:
Push Buttons and Operator Interface

Environment:
30mm, 9001K, 9001SK

Resolution:
Add Form Y243 to substitutes standard 9001KA1 contact block with reed contact block 9001KA51 in push-to-test pilot light so that it can be used in certain hazardous locations such as Class 1, Division 2.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings