Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement shaft for a 9421NW2 or 9421NW2B?
Issue:
Is there a replacement shaft for a 9421NW2 or 9421NW2B?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Class 9421 Circuit Breaker Operating Mechanism

Resolution:
9421NS16 is a 166mm shaft and 9421NS36 is a 360mm shaft. Either can be cut to length.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings