Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the dimensions for a QOFP filler plate?
Issue:
Product Design Features

Product Line:
QO load centers

Resolution:
QOFP is for current design QO load centers and some older style load centers with spaces measuring 0.75" x 2.31". If you have an older load centers with spaces measuring  0.75" x 2.44", the QO1FP would work.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings