Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use any panelboard rated 28 Vdc if I am only installing 20A circuit breakers?

Issue:
Panelboard to be used frated 28 VDC with 20A circuit breakers

Product Line:
NQ

Environment:
Application

Cause:
Selection

Resolution:
Square D suggests using a NQ panelboard. These are rated to 48 Vdc.
NF panelboards cannot be used in DC applications. I-Lines can be used up to 250 Vdc.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings