Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the mounting screws for a Powerpact L frame breaker?
Issue:
Replacement mounting screws for L Frame Breaker

Product Line:
Power Pact L-Frame Breaker

Resolution:
GHD11519AA is bag of 4 mounting screws. These screws are for all Powerpact L frame circuit breakers except for I-Line mounted, plug-in, and drawout.
This kit includes four bolts that are M5 x 85.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings