Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the NEMA Class 8502 contactor be converted to a Class 8536 starter by installing an overload relay?
Issue:
Overload needed to make a contactor into a starter

Product Line:
NEMA Contactors and Starters

Environment:
Type S contactors and Starters

Cause:
Contactor obtained when a starter is needed

Resolution:
The NEMA size 00, 0 & 1 contactors can be converted to starters by ordering and installing the appropriate replacement overload relay. However, due to baseplate differences between the contactor and starter on the NEMA size 2 and above, you cannot create a starter by combining a contactor and replacement overload. The closest we can get is to have a contactor with a separate mount overload.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings