Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an SC2040M200F, series M02?
Product Line:
CSED Combination Service Entrance Devices

Environment:
Applicable only to SC2040M200F, series M02

Resolution:
The repair parts numbers for the SC2040M200F, series M02, are shown in the below list. These are the parts that can be replaced. Other parts are not replaceable
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE
Meter Cover Assembly - 4053442852
Meter Cover Mounting Screw - 4020513001K (contains 10 screws; only one screw is required)
Branch Wiring Gutter Cover - 4056178101
Branch Wiring Gutter Cover Mounting Screw - 4020513001K (contains 10 screws; only one screw is required)
Utility Pullbox Cover - 4056181150 (includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - 4056181250
Load Center Cover Mounting Screws - (2) 2142217101
Dead Front Interior Trim - 7329420701
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only two screws are required)
Load Center Interior - 4056162050 (main breaker not included)
Load Center Interior Mounting Screw - (4) 4020510001 and (1) 4020510201
Main Breaker - QOM2200VH
Meter Base - 4052720650 (base only; line and load phase jaws not included)
Meter Base Mounting Screw - 2142717200
Meter Jaw - (4) 7329746450 (includes blade guides)
Meter Jaw Mounting Keps Nut - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Meter Sealing Ring - 2920910001
Left Line Side Phase Lug - 4025116051
Left Line Side Phase Lugs Mounting Bolt - 2271020242
Left Line Side Phase Lugs Mounting Keps Nut - 2342702001

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings