Issue:
What are the power requirements for a Micrologic 5 and 6 trip units for Powerpact H, J, L breakers?
Product Line:
Circuit Breakers
Environment:
Powerpact H, Powerpact J, Powerpact L circuit breakers
Cause:
It is necessary to adequately size control power transformers for the load they will serve
Resolution:
Each Micrologic 5.2, 5.3, 6.2, 6.3 trip unit requires 30 mA @ 24 Vdc.
What are the power requirements for a Micrologic 5 and 6 trip units for Powerpact H, J, L breakers?
Product Line:
Circuit Breakers
Environment:
Powerpact H, Powerpact J, Powerpact L circuit breakers
Cause:
It is necessary to adequately size control power transformers for the load they will serve
Resolution:
Each Micrologic 5.2, 5.3, 6.2, 6.3 trip unit requires 30 mA @ 24 Vdc.