Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which surge protective device is recommended for safeguarding a 480V Delta, 3-phase motor?
Issue:
Which surge protective device is recommended for safeguarding a 480V Delta, 3-phase motor?

Product Line:
Surge Protection Devices

Environment:
Motor load

Cause:
New product selection

Resolution:
It is recommended to utilize a surge protective device configured for a 480V Delta system and equipped with EMI/RFI filtering capabilities.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings