Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a control tap option for the Powerpact L lugs?

Product line:
Circuit Breakers

Environment:
Powerpact L frame only

Resolution:
Yes, control wire taps come standard with the Powerpact L frame lugs. It consists of a tapped hole in the face of the lug (screw not included).
For control wire installation, use an 8-32 x 1/4 in. screw (not provided) into tapped control wire hole in lower left hand corner of lug.

As an example of a Powerpact L frame breaker lug with hole for control tap wire, see the drawing below of the AL600LS52K3 lug.

Control Tap Lug

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings