Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the mounting height for Square D I-Line circuit breakers and subfeed lug kits?
Issue:
What is the mounting height (in inches) for the FY, FA, FH, SL-100, FI, HDA, HGA, HJA, HLA, QBA, QDA, QGA, QJA, JDA, JGA, JJA, JLA, LDA LGA LJA LLA LRA KI, SL250, LA, LH, SL400, LC, LI, LXI, MGA, MJA, MA, MH, SL800, PGA, PJA, PLA, RGA, RJA, AND RLA in an I-LINE panel?

Product Line:
I-LINE Breakers

Resolution:
See table below for mounting height for various breakers:
Frame Poles(in)
FD, FG, FJ11.5
FY, FA, FH, BD, BG, BJ, BK1
FA, FH, BD, BG, BJ23
FD, FG, FJ (no accessories)2, 3
HD, HG2
QB, QD, QG, QJ, Q22
FA, FH, SL100, BD, BG, BJ34.5
FC, FI2, 3
FD, FG, FJ (with accessories)2, 3
HD, HG3
HJ, HL, HR, QO Distribution Panels (HQO part numbers)2, 3
QB, QD, QG, QJ, Q23
JD, JG, JJ, JL, JR, KA, KH, KC, KI, IK, SL2502, 34.5
LA, LH, Q4, SL400, Smart Cell (ICW part numbers)6
LD, LG, LJ, LL, LR
LC, LI, LX, LXI, LE7.5
MG, MJ, MA, MH, MX, ME9
PG, PJ, PL
SL800, SL800M5, SL1200P5, SL1200P6, SL1200P7, S33931
IL12
RG, RJ, RL, RGC, RJC, RLC, S33930, NA, NC, NX, NE15


From page 9-34 in Section 9, Digest 177


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings