Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the door gasketing be obtained for a Nema 1A, NQ or NF panelboard enclosure?
Issue:
Loose gasketing material

Product Line:
Panelboards

Environment:
NQ, NF

Cause:
Repair

Resolution:
Yes, order part number 80106-507-01 and this will have to be ordered per foot. (so customer will need to specify total feet required when ordering, and order must be placed on the Peru Plant).
This goes on the back of the door so a trim with door is required. For a Nema 12 rating use a MH**WP box.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings