Issue:
Which GS fusible disconnect switches come with lugs?
Product Line:
GS1 and GS2
Environment:
US Product
Cause:
Some units come with lugs, and some units do not.
Resolution:
The following units come with lugs built in - these lugs are not replaceable (wire sizes are also specified):
GS1DDU3 - AWG #14 - #10
GS1DU3 - AWG #14 - #10
GS2EEU3 - AWG #14 - #10
GS2EU3N - AWG #14 - #6
GS2GU3N - AWG #10 - #6
GS2JU3N - AWG #12 - #1
The 200 amp and above can have lugs added in the field:
Which GS fusible disconnect switches come with lugs?
Product Line:
GS1 and GS2
Environment:
US Product
Cause:
Some units come with lugs, and some units do not.
Resolution:
The following units come with lugs built in - these lugs are not replaceable (wire sizes are also specified):
GS1DDU3 - AWG #14 - #10
GS1DU3 - AWG #14 - #10
GS2EEU3 - AWG #14 - #10
GS2EU3N - AWG #14 - #6
GS2GU3N - AWG #10 - #6
GS2JU3N - AWG #12 - #1
The 200 amp and above can have lugs added in the field:
Terminal Lugs
| For Use On: | Rating | No. of Wires per Lug | No. of Lugs per Terminal | Lug Size (AWG) | Wire Type | Lugs per Kit | Lug Kit |
|---|---|---|---|---|---|---|---|
| 30 | 1 | 1 | #12–2/0 | Cu | — | Standard | |
| 60 | 1 | 1 | #12–2/0 | Cu | — | Standard | |
| 100 | 1 | 1 | 6–300 kcmil | Cu/Al | 6 | ||
| 200 | 1 | 1 | 6–300 kcmil | Cu/Al | 6 | ||
| 400 | 2 | 1 | 350 MCM—6 | Cu/Al | 6 | ||
| 1 | 1 | 600 MCM—4 | Cu/Al | 6 | |||
| 2 | 250 MCM—1/0 | ||||||
| 600 | 2 | 1 | 2 x 2–600 kcmil | Cu/Al | 6 | ||
| 800 | 2 | 2 | 2 x 2–600 kcmil | Cu/Al | 12 | ||
| 1000 | 2 | 2 | 2 x 2–600 kcmil | Cu/Al | 12 | ||
| 1200 | 2 | 2 | 2 x 2–600 kcmil | Cu/Al | 12 | ||
| 30 | 1 | 1 | #14–#10 | Cu | — | Standard | |
| 30 | 1 | 1 | #14–#10 | Cu | — | Standard | |
| 30 | 1 | 1 | #14–#10 | Cu | — | Standard | |
| 30 | 1 | 1 | #14–#6 | Cu | — | Standard | |
| 60 | 1 | 1 | #10–#6 | Cu | — | Standard | |
| 100 | 1 | 1 | #12–#1 | Cu | — | Standard | |
| 200 | 1 | 1 | 6–300 kcmil | Cu/Al | 6 | ||
| 400 | 2 | 1 | 350 MCM—6 | Cu/Al | 6 | ||
| 1 | 1 | 600 MCM—4 | Cu/Al | 6 | |||
| 2 | 250 MCM—1/0 | ||||||
| 600 | 2 | 1 | 2 x 2–600 kcmil | Cu/Al | 6 | ||
| 800 | 2 | 1 | 2 x 2–600 kcmil | Cu/Al | 6 |