Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use an XW6848+ and an XW6048 in a dual setup?
Can I use an XW6848+ and an XW6048 in a dual setup?

Request:Customer has(1) XW6048 and is looking to install an additional inverter which would be the XW6848+

Solution:  This can be done, but they would have to downgrade the firmware on the XW6848+ to an XW6048 or
upgrade the XW6048 to XW+NA6848 firmware

NOTE:Please see attachment for details

Schneider Electric Canada

Attachment(s)
Technical Note-XW-XW+ Compatibility(976-0316-01-01_Rev-A).pdf [129.54 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings