Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where are the weep or drain holes in a NEMA 3r I-Line panel?

Issue:
Location of the drain holes in a NEMA 3r I-Line box

Product Line:
Panelboards

Environment:
NEMA 3R Outdoor rated I-Line panelboards

Cause:
Moisture drainage

Resolution:
In the bottom endwall there are 2 holes with screws in them. For NEMA 3R remove the screws to allow for drainage. For a NEMA 5 or 12 dust proof rating leave the screws in.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings