Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the coil consumption of an LC1D50 with an LA4DFB interface module attached?
Issue:
Coil consumption when LA4DFB used in Tesys D LC1D50 contactor

Product Line:
TeSys D-Line Contactors

Environment:
All Product Lines

Resolution:
With the LA4DFB attached to the LC1D50, the coil consumption is 25mA.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings