Issue:
Insulation class of the coils used with the NEW TESYS 'D' range D09 to D150.
Product Line:
TESYS D, LC1D09 - LC1D150
Environment:
Unique to the LC1D product line
Insulation class of the coils used with the NEW TESYS 'D' range D09 to D150.
Product Line:
TESYS D, LC1D09 - LC1D150
Environment:
Unique to the LC1D product line
Cause:
Insulation class for product knowledge
Resolution
The class of the wires of the contactor coils is H
The rated insulation voltage is : 690V up to LC1D32
( remark : today for contactors from LC1D40 to LC1D150 ) there is not electrical characteristic changes according to the D2 line
Released for: Schneider Electric Canada