Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find documentation for the EM35xxA series meter?
Product Line
EM35xxA series meter

Resolution
Both the EM35xx[A] and EM35xx series meters operate identically. Documentation for the EM35xx series meter can be used for the EM35xx[A] series. The only difference between the EM35xx and EM35xx[A] is the circuitry for the current input.

NOTE: Refer to article FA233732 for part numbering and supported CTs for the EM35xx[A] series meter.

For the Technical Guide, consider the EM35xxA a subset of the EM35xx series meter.
Review the attached documentation for the EM35xx series meter or visit FA212707 for additional documentation.

Schneider Electric Canada

Attachment(s)
EM3500 Technical Data Sheet.pdf [1.22 MB]
EM35xx_quick_start.pdf [1.57 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings