Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a current Powerpact I-line breaker be used in place of an obsoleted bolt on I-line breaker in the I line panel?

Article available in these languages: Spanish

Issue:
Will the current I-line breakers install in the same place as an obsolete bolt-on I-line breaker?

Product Line:
I Line Panelboard

Environment:
I-line Circuit Breakers

Resolution:
The current I line plug on breakers can be used in place of an obsoleted I line breaker with the Bolt-on feature, ie, KAB34225, but does not have this bolt on feature. The I-line jaws , for both breakers, are of the same design.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings