Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the SC3042M225PF, Series M01?
Issue:
Current Design Repair Parts

Product Line:
Combination Service Entrance Devices

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4053442852
Meter Cover Mounting Screw - 4020513001K (contains 10 screws; only one screw is required to secure the cover)
Branch Wiring Gutter Cover (Below Meter Cover) - 4056178101
Branch Wiring Gutter Cover Mounting Screw - 4020513001K (contains 10 screws; only one screw is required to secure the cover)
Utility Pullbox Cover - 4056181150 (includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - MTR10570 (includes hinges)
Load Center Cover Mounting Screws - 2142217101 (2 required)
Dead Front Interior Trim - EAV67728
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only two screws are required to secure the interior trim)
Load Center Interior - MTR10002 (main breaker and large neutral lugs not included)
Load Center Interior Mounting Screw - 4020510001 (2 required)
Main Breaker - QOM2225VH
Main Breaker mounting keps nut - 2342702001 (2 required; attaches the load side of MB to studs in main bus bars)
Meter Base - 4054102503 (phenolic base only - does not include line and load phase jaws, see below. If 5th jaw is required order catalog number 5J)
Meter Base Mounting Screw - 2142717200
Meter Socket Jaw - 7329794850 (4 required for complete meter socket; blade guide not included)
Meter Jaw Mounting Keps Nut - 2342702001 (one PER meter jaw)
Meter Jaw Blade Guide - 4052761901 (one PER meter jaw)
Meter Jaw with Blade Guide - 7329746450 (4 required for complete meter socket and includes blade guide)
Meter Sealing Ring - 2920910001
Left Line Side Phase Lug - 4025116051
Left Line Side Phase Lugs Mounting Bolt - 2271020242
Left Line Side Phase Lugs Mounting Keps Nut - 2342702001
NOTES:
1) WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE
2) The device comes standard with five large branch neutral lugs; two of part number LK70AN, one of part number 4025130250, one of part number LK100AN, and one of part number LK125AN; IF NEEDING REPLACEMENTS, ORDER SEPARATELY.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings