Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the wire bending clearances for the HCP-SU I-Line interior with HC2686DB box (NEMA 1) or HC2886WP enclosure (NEMA 3R) ?
Issue:
What are the wire bending clearances for the HCP-SU , single row I Line interior with HC2686DB box ?

Product Line:
I Line Panelboards

Environment:
Installation

Cause:
Clearance

Resolution:
Gutter space for either left , or right hand breaker orientation of the HCPSU interior, will be 9.8 inches for Nema 1 boxes ,and 10.8" for 3R boxes.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings