Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In an Ethernet Daisy Chain, will downstream meters still communicate if a meter loses power?

Issue
In an Ethernet Daisy Chain, will downstream meters still communicate if a meter loses power?

Product Line
PM8000, PM5500, ION9000, ION8650, ION7650

Environment
PowerLogic meters with multiple Ethernet ports

Cause
Unlike a serial daisy chain, if a meter in an Ethernet Daisy Chain loses power, all devices downstream of the device will lose communications. This is due to the meter also containing a network switch which needs to remain powered in order for traffic to pass through.

Resolution
To ensure that there are no comms loss due to power outage on Ethernet devices, a UPS can be installed to ensure that the meter does not power off during a service interrupt.

For the maximum number of devices that can be cascaded (daisy chained) via the Ethernet port of a PM5500/PM8000, please refer to FA234113.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings