Issue:
Product Design Features
Product Line:
QO or Homeline Load Centers
Resolution:
The LK125AN branch neutral/ground lug will install on one of the branch neutral bars of the load center interior or can be installed on a PK__GTA ground bar installed in the load center.
The LK125AN will mount under two(2) wire binding screws of the branch neutral bar and will accept (1) #14 - 2/0 AL/Cu wire.
The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.
A PDF copy of the complete instructions is attached below the video.

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Remove Cover from load center.
3) Insert the Lug Tangs A through the cutout slot in the black insulator B, so the insulator will now be around the lug and only the tangs will be exposed.
NOTE: The lug is mounted to a small plate that has Tangs on one side of the plate and the Tangs need to be inserted into the slot in the black insulator before inserting them into the branch neutral bar.
4) Loosen 2 adjacent wiring binding screws C in the branch neutral bar D.
5) Insert the Lug Tangs into the 2 holes under the Loosened wire binding screws from step 4.
6) Tighten the wiring binding screws to 30 lb-in (3.4 N-m)
7) Install the appropriate wire size to be used in the Lug and refer to Table 1, on page 1 of the instructions for torque.
NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.
Product Design Features
Product Line:
QO or Homeline Load Centers
Resolution:
The LK125AN branch neutral/ground lug will install on one of the branch neutral bars of the load center interior or can be installed on a PK__GTA ground bar installed in the load center.
The LK125AN will mount under two(2) wire binding screws of the branch neutral bar and will accept (1) #14 - 2/0 AL/Cu wire.
The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.
A PDF copy of the complete instructions is attached below the video.
Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Remove Cover from load center.
3) Insert the Lug Tangs A through the cutout slot in the black insulator B, so the insulator will now be around the lug and only the tangs will be exposed.
NOTE: The lug is mounted to a small plate that has Tangs on one side of the plate and the Tangs need to be inserted into the slot in the black insulator before inserting them into the branch neutral bar.
4) Loosen 2 adjacent wiring binding screws C in the branch neutral bar D.
5) Insert the Lug Tangs into the 2 holes under the Loosened wire binding screws from step 4.
6) Tighten the wiring binding screws to 30 lb-in (3.4 N-m)
7) Install the appropriate wire size to be used in the Lug and refer to Table 1, on page 1 of the instructions for torque.
NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.
Released for: Schneider Electric Canada