Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are combination arc fault breakers available in Federal Pioneer Stab-lok?
Issue:
Can you get combination AFI breakers for Federal Pioneer Stab-lok panels?

Product Line:
Loadcentres

Resolution:
We do not offer combination AFI breakers for Stab-lok panels. To add new AFI breakers, you would need to put in a subpanel or replace the existing panel with a new panel.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings