Issue:
There are two ways to mount the LK4AH0110CN, LK4AH0120CN, LK4AH0410CN, and LK4AH0420CN. Is the NEMA rating affected by the different mounting methods?
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
IEC LK4 Disconnect switches
Cause:
Product Application
Resolution:
Either way handle is mounted, the NEMA 4 rating is maintained.
There are two ways to mount the LK4AH0110CN, LK4AH0120CN, LK4AH0410CN, and LK4AH0420CN. Is the NEMA rating affected by the different mounting methods?
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
IEC LK4 Disconnect switches
Cause:
Product Application
Resolution:
Either way handle is mounted, the NEMA 4 rating is maintained.
Released for: Schneider Electric Canada