Issue:
Can a 225A neutral assembly NQNL2 be used instead of the 100A neutral assembly NQNL1 for an NQ 100A panel?
Product Line:
Panelboards
Environment:
NQ 100% and 200% neutrals
NQNL2, NQNL1
Resolution:
No. The neutral assemblies are UL listed and tested for use in the proper ampere rated panels. The UL labeling
will be incorrect and may void the UL listing of the panel.
Can a 225A neutral assembly NQNL2 be used instead of the 100A neutral assembly NQNL1 for an NQ 100A panel?
Product Line:
Panelboards
Environment:
NQ 100% and 200% neutrals
NQNL2, NQNL1
Resolution:
No. The neutral assemblies are UL listed and tested for use in the proper ampere rated panels. The UL labeling
will be incorrect and may void the UL listing of the panel.
Released for: Schneider Electric Canada