Issue:
Product design features
Product Line:
Circuit Breaker Enclosure
Environment:
Padlocking
Cause:
Application
Resolution:
Yes, the H150F and H150S are provided with a hasp welded to the cover to enable installing a padlock that will block the travel of the circuit breaker handle from the OFF or ON position.
Product design features
Product Line:
Circuit Breaker Enclosure
Environment:
Padlocking
Cause:
Application
Resolution:
Yes, the H150F and H150S are provided with a hasp welded to the cover to enable installing a padlock that will block the travel of the circuit breaker handle from the OFF or ON position.
Released for: Schneider Electric Canada